MKD-C "ND" Central Power Supply Variant
The MKD-C "ND" is a central power supply variant introduced in 2022 with a substitute chip.
It is identified with "-NC" in the part number:
MKD-Cxxxxxx-NDEC-xxxx
Contact your local Kollmorgen representative for more information about the drive.
FAQs for the "ND" Central Power Supply
AKD firmware v01-22-00-000 and later support the "ND" central power supply.
KAS IDE "Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger v4.00 and later are compatible.
Kollmorgen recommends using v4.00 and later because the features available in AKD firmware v01-22 are integrated with and supported by KAS IDE v4.00.
The MKD-C “ND” support was introduced in KAS IDE v4.00 with AKD firmware v01-22.
Previous MKD-C central power supplies are not supported.
The AKD firmware and KAS firmware packages are available in the downloads section of Kollmorgen website.
Previous models are not supported and should not be swapped with the “ND” model.
Kollmorgen recommends using MKD-C "ND" central power supply for new machines.