Backup and Restore a AKD PDMM or PCMM

The SD card is used for backing up and restoring the data from a AKD PDMM or PCMM.

Backup

Backup is performed with one of these methods:


  • For a complete backup of both the controller and drive, use the Web Server backup.

Restore

Restoring information to the controller is performed with one of these methods. Both methods restore the controller (and AKD PDMM drive) with whatever was saved to the SD card.

Backup & Restore What? To/From SD card via B2/B3 buttons To/From SD card via Web Server
Controller: Firmware
Controller: Network Configuration
Controller: PLC Application
Controller: Retain Variables
EtherCAT Devices: Network Topology
EtherCAT Devices: AKD Drive Firmware
EtherCAT Devices: AKD Drive Parameters

Restore only

Data Transfer

  • The 7-segment display shows the chasing lights animation while the backup or restore is occurring.
  • The Backup and Restore functions have an all-or-nothing behavior.
    • If there is no SD card inserted, not enough space on the card, or if files are missing, nothing is copied and the 7-segment display shows an error code.
  • If files already exist on the SD card (in the backup directory), they are deleted and replaced with the new AKD PDMM or PCMM backup configuration files.
    • The files on the controller are replaced with the SD files.

  • Do not modify the files on the SD card because this could result in the restore function failing.


  • If there are multiple AKD PDMM or PCMM backup configurations, you must use one SD card per backup configuration.