Using the KAS Web Server

Kollmorgen Automation Suite™ comes with a web server that allows you to perform the following operations:

The web server may be accessed two ways:

  1. Open a web browser and enter the controller's IP address.
  2. From the Controller node in the Project tree in the KAS IDEClosed "Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger.
    • Double-click the Controller node
    • Select "Access Webserver" from the right-mouse menu.

  • If you do not know the IP address assigned to the controller:

    1. Press B3 once.
      The 7-segment display flashes the letters I and P.
    2. Press B2 to select the IP option.
      The 7-segment display shows the IP address.

The web server consists of the home page, and the KAS Application, Settings, Backup & Restore, Diagnostics and Help tabs. The Help tab is a link which opens the Web Server manual.

Figure 6-4: The Webserver Tabs as seen on an AKD PDMM webserver.