Restore tab

Restore Controller

This function restores an AKD PDMM or PCMM's firmware, network configuration, retained variables, user data, and PLCClosed "Programmable Logic Controller" A Programmable Logic Controller, PLC, or Programmable Controller is a digital computer used for automation of industrial processes, such as control of machinery on factory assembly lines. Used to synchronize the flow of inputs from (physical) sensors and events with the flow of outputs to actuators and events application from the SD card.

PCMM2G

This function restores PCMM2G’s firmware, network configuration, retained variables, user data, and PLC application from the USBClosed "Universal Serial Bus" USB is a serial bus standard to interface devices flash drive.

Restore EtherCAT Devices

This function automatically restores the data and firmware of any replaced AKD or AKD2G drives and the station alias of other EtherCAT devices.

Advanced

Click this button to create a map of the network and its components.

  • If a valid firmware file is found, and the current topology matches the backup file, select the devices that need to be restored.
  • Click Restore EtherCAT Devices restores the drive's firmware.