EtherCAT Toolbar

Each icon in this toolbox has a brief explanation provided below in order to explain the functionality.

EtherCAT Toolbar Icons
Icon Name Description
Online Configuration Mode

This action is only available when the KAS RuntimeClosed In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running is connected with the target Controller.