BlinkA

PLCopen motion icon

 Function BlockClosed A function block groups an algorithm and a set of private data. It has inputs and outputs. - Asymmetric blinker.

Inputs

Input

Data Type

Range

Unit

Default

Description

RUN

BOOL

 

 

 

Enabling command.

TM0

TIME

 

 

 

Duration of FALSE state on output.

TM1

TIME

 

 

 

Duration of TRUE state on output.

Outputs

Output

Data Type

Range

Unit

Description

Q

BOOL

 

 

Output blinking signal.

Time Diagram

Remarks

  • The output signal is FALSE when the RUN input is FALSE.

FBD Language

FFLD Language

  • In the FFLD language, the input rung is the IN command.
    • The output rung is the Q output.

IL Language

(* MyBlinker is a declared instance of BLINKA function block *)
Op1: CAL MyBlinker (RUN, TM0, TM1)
     FFLD  MyBlinker.Q
     ST  Q

ST Language

(* MyBlinker is a declared instance of BLINKA function block. *)
MyBlinker (RUN, TM0, TM1);
Q := MyBlinker.Q;

See Also