DTGetNTPSync

 Function BlockClosed A function block groups an algorithm and a set of private data. It has inputs and outputs. - Read the NTPClosed "Network Time Protocol" A networking protocol for clock synchronization between computer systems. The PCMM2G can be configured to synchronize with public NTP time servers over the internet or a local NTP time server for networks that are not connected to the internet. synchronization enable state.

This function block is specific for PCMM2G only.

Inputs

Input

Data Type

Range

Unit

Default

Description

Execute

BOOL

TRUE, FALSE

N/A

No default

If TRUE, request to read the synchronization enable state.

Outputs

Output

Data Type

Range

Unit

Description

Done

BOOL

TRUE, FALSE

N/A

If TRUE, the command completed successfully.

Error

BOOL

TRUE, FALSE

N/A

If TRUE, an error has occurred.

ErrorID

DINT

No range

N/A

Indicates the error if the Error output is set to TRUE.

Error Codes

  • 23 = Internal error. See controller log for details.
  • 15000 = Controller type does not support this function block.

SynchEn

BOOL

TRUE, FALSE

N/A

The present NTP synchronization state.

  • TRUE = synchronization enabled.
  • FALSE = synchronization disabled.

Remarks

None

FBD Language

FFLD Language

IL Language

Not available.

ST Language

// read the NTP synchronization state
Inst_DTGetNTPSync( bGetNTPSync );
if Inst_DTGetNTPSync.Done then
   bGetNTPSync := false;

   if NOT Inst_DTGetNTPSync.Error then
      bNTPSyncEnable := Inst_DTGetNTPSync.SynchEn;
   else
      ErrorID := Inst_DTGetNTPSync.ErrorID;
   end_if;
end_if;

See Also