DTSetTimeZone

 Function BlockClosed A function block groups an algorithm and a set of private data. It has inputs and outputs. - Set the time zone.

This function block is specific for PCMM2G only.

Inputs

Input

Data Type

Range

Unit

Default

Description

Execute

BOOL

TRUE, FALSE

N/A

No default

If TRUE, request to set the time zone.

TimeZone

STRING

No range

N/A

No default

The time zone the controller should use.

Outputs

Output

Data Type

Range

Unit

Description

Done

BOOL

TRUE, FALSE

N/A

If TRUE, the command completed successfully.

Error

BOOL

TRUE, FALSE

N/A

If TRUE, an error has occurred.

ErrorID

DINT

No range

N/A

Indicates the error if the Error output is set to TRUE.

Error Codes

  • 23 = Internal error. See controller log for details.
  • 15000 = Controller type does not support this function block.
  • 16201 = Invalid time zone.

Remarks

None

FBD Language

FFLD Language

IL Language

Not available.

ST Language

// configure the time zone
Inst_DTSetTimeZone( bSetDTZone, TimeZone );
if Inst_DTSetTimeZone.Done then
   bSetDTZone := false;

   bError := Inst_DTSetTimeZone.Error;
   ErrorID := Inst_DTSetTimeZone.ErrorID;
end_if;

See Also