eipReadAttr

PLCopen motion icon

 Function BlockClosed A function block groups an algorithm and a set of private data. It has inputs and outputs. - sends an explicit message (UCMM) to an EtherNet/IP adapter, for reading a single CIPClosed "Common Industrial Protocol " The Common Industrial Protocol allows complete integration of control with information, multiple CIP Networks, and Internet technologies attribute.

Inputs

Input

Data Type

Range

Unit

Default

Description

Attr

UINT

 

 

 

Identifier of the CIP attribute.

Class

UINT

 

 

 

Class identifier of the CIP object.

Data

array of UINT

     

Buffer where to store the received data. If the actual attribute length is greater than the size of this array, value will be truncated when read.

Inst

UINT

 

 

 

Instance identifier of the CIP object.

SrvIP

STRING

 

 

 

IP address of the server (adapter) (e.g., configured in the EtherNet/IP Scanner configuration).

Snd

BOOL

 

 

 

A rising edgeClosed A rising edge is the transition of a digital signal from low to high. It is also called positive edge on this input starts the exchange.

The DONE output signals the end of exchange.

Outputs

Output

Data Type

Range

Unit

Description

Done

BOOL

 

 

This output is TRUE during one cycle when the exchange is finished, whether the exchange succeeded or failed.

Warning: This output can be TRUE just after the call to block when starting a new exchange in case of invalid parameters.

EmErr

UINT

 

 

In case of a UCMM error, this is the CIP general status error code.

EmErrExt

UINT

 

 

In case of a UCMM error, this is the CIP extended status error code.

Err

UINT

 

 

Main error report.

Can be one of these values:
0 = no error.
1 = invalid input arguments.
2 = system is busy (see remarks).
3 = timeout waiting for the answer (the timeout value is 3 seconds).
4 = UCMM error was returned by the server others = internal errors (reserved for technical support).

RcvSize

UINT

 

 

Actual size of the CIP attribute answered by the server.

If this size is greater than the size of the DATA input array, it indicates the value was truncated.

Remarks

  • The CIP instance number can be 16-bits [1...65535].
  • The servers (adapters) accessed by this block must be configured in the EtherNet/IP Scanner fieldbus configuration.
  • Only one explicit message (read or write) can be sent at one time to the same server.
    • If another message is pending you receive the error report 3 (busy) after calling the block to start a new exchange.
  • Consider SerializeIn and SerializeOut functions for extracting data from the read buffer.

FBD Language

Not available.

FFLD Language

Not available.

IL Language

Not available.

ST Language

// used variables
// Inst_eipReadAttr : eipReadAttr ;
// bRead : BOOL ; (* request for READ *)
// DataRead : ARRAY [0 .. 15] OF USINT ; (* read data *)
// Server identification and CIP things

#define SRVIP '192.168.33.21'
#define CLASSID UINT#100
#define INSTID_READ UINT#1
#define ATTRID UINT#3
/////////////////////////////////////////////////////////////////////////////////////////
// requested READ command

if bRead then
Inst_eipReadAttr (bRead, SRVIP, CLASSID, INSTID_READ, ATTRID, DataRead);
end_if;
// READ answer here ?
if Inst_eipReadAttr.Done then
// check answer - if OK answered data is in DataRead array
if Inst_eipReadAttr.Err = 0 then
printf ('READ ok - size = %lu bytes',
any_to_dint (Inst_eipReadAttr.RcvSize));
else
printf ('READ Error %lu (UCMM Error %lu, %lu)',
any_to_dint (Inst_eipReadAttr.Err),
any_to_dint (Inst_eipReadAttr.EmErr),
any_to_dint (Inst_eipReadAttr.EmErrExt));
end_if;
// reset READ command and block input
Inst_eipReadAttr (false, SRVIP, CLASSID, INSTID_READ, ATTRID, DataRead);
bRead := false;
end_if;

See Also