EnableEvents

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Enable or disable the production of events for binding (runtimeClosed In computer science, runtime (or run-time) describes the operation of a computer program, the duration of its execution, from beginning to termination (compare compile time). Within KAS, runtime also refers to the virtual machine that manage the program written in a computer language while it is running to runtime variable exchange).

Inputs

Input

Data Type

Range

Unit

Default

Description

EN

BOOL

 

 

 

  • TRUE to enable events.
  • FALSE to disable events.

Outputs

Output

Data Type

Range

Unit

Description

ENO

BOOL

 

 

Echo of EN input.

Remarks

  • Production is enabled when the application starts.
  • The first production is operated after the first cycle.
  • To disable events since the beginning, you must call EnableEvents (FALSE) in the very first cycle.

FBD Language

FFLD Language

  • In FFLD language, the input rung (EN) enables the event production.
    • The output rung keeps the state of the input rung.
    • Events are enables if EN is TRUE.
    • ENO has the same value as EN.

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  EN
     EnableEvents
     ST  ENO

ST Language

ENO := EnableEvents (EN);

See Also

Alarm_A