LoWord

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Get the lowest word of a double word.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

UDINT

 

 

 

32-bit register.

Outputs

Output

Data Type

Range

Unit

Description

Q

UINT

 

 

Lowest significant word.

Remarks

None

FBD Language

FFLD Language

  • In the FFLD language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
  • The function is executed only if EN is TRUE.
  • ENO keeps the same value as EN.

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  IN
     LOWORD
     ST  Q

ST Language

Q := LOWORD (IN);

See Also