Alarm_M

PLCopen motion icon

 Function BlockClosed A function block groups an algorithm and a set of private data. It has inputs and outputs. - Alarm with manual reset.

Inputs

Input

Data Type

Range

Unit

Default

Description

ACK

BOOL

 

 

 

Acknowledge command.

IN

BOOL

 

 

 

Process signal.

RST

BOOL

 

 

 

Reset command.

Outputs

Output

Data Type

Range

Unit

Description

Q

BOOL

 

 

TRUE if alarm is active.

QACK

BOOL

 

 

TRUE if alarm is acknowledged.

Remarks

  • Combine this block with the lim_alrm block for managing analog alarms.

Sequence

FBD Language

FFLD Language

IL Language

(* MyALARM is declared as an instance of ALARM_M function block *)
Op1: CAL MyALARM (IN, ACK, RST)
FFLD  MyALARM.Q
STClosed "Structured text" A high-level language that is block structured and syntactically resembles Pascal  Q
FFLD  MyALARM.QACK
ST  QACK

ST Language

(* MyALARM is declared as an instance of ALARM_M function block *)
MyALARM (IN, ACK, RST);
Q := MyALARM.Q;
QACK := MyALARM.QACK;

See Also

Alarm_A