SetWithin

.PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Force a value when inside an interval.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

ANY

 

 

 

Input.

MIN

ANY

 

 

 

Low limit of the interval.

MAX

ANY

 

 

 

High limit of the interval.

VAL

ANY

 

 

 

Value to apply when inside the interval.

Outputs

Output

Data Type

Range

Unit

Description

Q

ANY

 

 

Result.

Truth Table

In

Q

IN < MIN

IN

IN > MAX

IN

MIN < IN < MAX

VAL

Remarks

  • The output is forced to VAL when the IN value is within the [MIN ... MAX] interval.
  • It is set to IN when outside the interval.