ATOH

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Converts string to integer using hexadecimal basis.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

STRING

 

 

 

String representing an integer in hexadecimal format.

Outputs

Output

Data Type

Range

Unit

Description

Q

DINT

 

 

Integer represented by the string.

Truth Table

IN

Q

''

0

'12'

18

'a0'

160

'A0zzz'

160

Remarks

  • The function is case insensitive.
  • The result is 0 (zero) for an empty string.
  • The conversion stops before the first invalid character.

FBD Language

AtoH FBD Language Block

FFLD Language

  • In the FFLD language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.

AtoH FFLD Language Block

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  IN
     ATOH
     ST  Q

ST Language

Q := ATOH (IN);

See Also

HTOA