any_to_time

PLCopen motion icon

Operator - Converts the input into time value.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

ANY

 

 

 

Input value.

Outputs

Output

Data Type

Range

Unit

Description

Q

TIME

 

 

Value converted to time.

Remarks

  • For BOOL input data types, the output is t#0ms or t#1ms.
  • For DINT or REAL input data type, the output is the time represented by the input number as a number of milliseconds.
  • For STRING input data types, the output is the time represented by the string or t#0ms if the string does not represent a valid time.

FBD Language

Any_To_TimeFbd.gif (1272 octets)

FFLD Language

  • In the FFLD language, the conversion is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.

Any_To_TimeLd.gif (1498 octets)

IL Language

Op1: FFLD  IN
ANY_TO_TIME
ST  Q

ST Language

Q := ANY_TO_TIME (IN);

See Also