ascii

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Get the ASCII code of a character within a string.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

STRING

 

 

 

Input string.

POS

DINT

 

 

 

Position of the character within the string.

The first valid position is 1.

Outputs

Output

Data Type

Range

Unit

Description

CODE

DINT

 

 

ASCII code of the selected character or 0 (zero) if position is invalid.

Remarks

None

FBD Language

FFLD Language

  • In the FFLD language, the input rung (EN) enables the operation.
    • The output rung (ENO) keeps the same value as the input rung.

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them       IN
     AND_MASK MSK
     ST       CODE

ST Language

CODE := ASCII (IN, POS);

See Also

char