bin_to_bcd

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Converts a binary value to a BCD (Binary Coded Decimal) value.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

DINT

 

 

 

Integer value.

Outputs

Output

Data Type

Range

Unit

Description

Q

DINT

 

 

Value converted to BCD or 0 if IN is less than 0.

Truth Table

IN

Q

-2

0 (invalid)

0

0

10

16 (16#10)

22

34 (16#22)

Remarks

  • The input must be positive.

FBD Language

FFLD Language

  • In the FFLD language, the operation is executed only if the input rung (EN) is TRUE. 
    • The output rung (ENO) keeps the same value as the input rung.

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them         IN
     BIN_TO_BCD
     ST         Q

ST Language

Q := BIN_TO_BCD (IN);

See Also

bcd_to_bin