expt

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Calculates a power.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

REAL

 

 

 

Real value.

EXP

DINT

 

 

 

Exponent.

Outputs

Output

Data Type

Range

Unit

Description

Q

REAL

 

 

Result: IN at the EXP power

Remarks

The exponent (second input of the function) must be the operand of the function.

FBD Language

PowFbd.gif (1241 octets)

FFLD Language

  • In the FFLD language, the conversion is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.
    • The function is executed only if EN is TRUE.
    • ENO keeps the same value as EN.

PowLd.gif (1506 octets)

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them   IN
     EXPT EXP
     ST   Q    (* Q is: (IN ** EXP) *)

ST Language

Q := EXPT (IN, EXP);

See Also