f_trig

PLCopen motion icon

 Function BlockClosed A function block groups an algorithm and a set of private data. It has inputs and outputs. - Falling pulse detection.

Inputs

Input

Data Type

Range

Unit

Default

Description

CLK

BOOL

 

 

 

Boolean signal.

Outputs

Output

Data Type

Range

Unit

Description

Q

BOOL

 

 

TRUE when the input changes from TRUE to FALSE.

Truth Table

CLK

CCLK (prev)

Q

0

0

0

0

1

1

1

0

0

1

1

0

Remarks

FBD Language

F_Trig FBD

FFLD Language

  • In the FFLD language, ]P[ and ]N[ contacts can be used.

F_Trig FFLD

IL Language

(* MyTrigger is declared as an instance of F_TRIG function block *)
Op1: CAL MyTrigger (CLK)
LDClosed "Ladder diagram" Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  MyTrigger.Q
ST  Q

ST Language

(* MyTrigger is declared as an instance of F_TRIG function block. *)
MyTrigger (CLK);
Q := MyTrigger.Q;

See Also

r_trig