FatalStop

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Breaks the cycle and stop with fatal error.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN

BOOL

 

 

 

Condition.

Outputs

Output

Data Type

Range

Unit

Description

Q

BOOL

 

 

TRUE if performed.

Remarks

  • This function breaks the current cycle and sets the Virtual Machine in ERROR mode.
    • Restarting normal execution is performed using the debugger.
  • The VM is stopped only if the IN argument is TRUE.
    • The end of the current cycle is then not performed.

FBD Language

Not available.

FFLD Language

Not available.

IL Language

Not available.

ST Language

Not available.

See Also