Programming Languages

This section provides information about the syntax, structure, and use of declarations and statements supported by the KAS IDEClosed "Integrated development environment" An integrated development environment is a type of computer software that assists computer programmers in developing software. IDEs normally consist of a source code editor, a compiler and/or interpreter, build-automation tools, and a debugger application language.

These are the available programming languages of the IECClosed "International Electrotechnical Commission" IEC is a not-for-profit, non-governmental international standards organization that prepares and publishes International Standards for all electrical, electronic and related technologies 61131-3 standard:

A language must be selected for each program or User-Defined Function Block of the application.

See these pages about the IEC 61131-3 programming languages: