<   LT

PLCopen motion icon

Operator - Test if first input is less than second input.

Inputs

IN1 : ANY   First input.
IN2 : ANY   Second input.

Outputs

Q : BOOL    TRUE if IN1 < IN2.

Remarks

Both inputs must have the same data type. In FFLD language, the input rung (EN) enables the operation, and the output rung is the result of the comparison. In ILClosed "Instruction list" This is a low-level language and resembles assembly language, the LT instruction performs the comparison between the current result and the operand. The current result and the operand must have the same datatype.

Comparisons can be used with strings. In that case, the lexical order is used for comparing the input strings. For instance, "ABC" is less than "ZX" ; "ABCD" is greater than "ABC".

ST Language

Q := IN1 < IN2;

FBD Language

LtFbd.gif (1226 octets)

FFLD Language

(* The comparison is executed only if EN is TRUE. *)
LtLd.gif (1443 octets)

IL Language

Op1: FFLD  IN1
     LT  IN2
     ST  Q    (* Q is true if IN1 < IN2 *)

See Also