ROOTPLCopen motion icon

FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Calculates the Nth root of the input.

Inputs

IN : REAL Real value.

N : DINT Root level.

Outputs

Q : REAL Result: Nth root of IN.

Remarks

ST Language

Q := ROOT (IN, N);

FBD Language

FFLD Language

(* The function is executed only if EN is TRUE *)
(* ENO keeps the same value as EN *)

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them  IN
     ROOT N
     STClosed "Structured text" A high-level language that is block structured and syntactically resembles Pascal   Q    (* Q is: ROOT (IN) *)