SR

PLCopen motion icon

 Function BlockClosed A function block groups an algorithm and a set of private data. It has inputs and outputs. - Set dominant bistable.

Inputs

Input

Data Type

Range

Unit

Default

Description

SET1

BOOL

 

 

 

Condition for forcing to TRUE.

Highest priority command.

RESET

BOOL

 

 

 

Condition for forcing to FALSE.

Outputs

Output

Data Type

Range

Unit

Description

Q

BOOL

 

 

Output to be forced.

Truth Table

SET1

RESET

Q1 prev

Q1

0

0

0

0

0

0

1

1

0

1

0

0

0

1

1

0

1

0

0

1

1

0

1

1

1

1

0

1

1

1

1

1

Remarks

  • The output is unchanged when both inputs are FALSE.
  • When both inputs are TRUE, the output is forced to FALSE. (set dominant)

FBD Language

SrFbd.gif (1307 octets)

FFLD Language

  • The SET1 command is the rung.
    • The rung is the output.

SrLd.gif (1460 octets)

IL Language

(* MySR is declared as an instance of SR function block *)
Op1: CAL MySR (SET1, RESET)
     FFLD  MySR.Q1
     ST  Q1

ST Language

(* MySR is declared as an instance of SR function block *)
MySR (SET1, RESET);
Q1 := MySR.Q1;

See Also