StringToArray / StringToArrayU

PLCopen motion icon

 FunctionClosed A function calculates a result according to the current value of its inputs. A function has no internal data and is not linked to declared instances. - Copies the characters of a STRING to an array of SINT.

Inputs

Input

Data Type

Range

Unit

Default

Description

DST

SINT

 

 

 

Destination array of SINT small integers.

USINT for StringToArrayU.

SRC

STRING

 

 

 

Source STRING.

Outputs

Output

Data Type

Range

Unit

Description

Q

DINT

 

 

Number of characters copied.

Remarks

This function:

  • Copies the characters of the SRC string to the first characters of the DST array.
  • Checks the maximum size destination arrays and reduces the number of copied characters if necessary.

FBD Language

FFLD Language

  • In the FFLD language, the operation is executed only if the input rung (EN) is TRUE.
    • The output rung (ENO) keeps the same value as the input rung.

IL Language

Op1: LDClosed "Ladder diagram"
Ladder logic is a method of drawing electrical logic schematics. It is now a very popular graphical language for programming Programmable Logic Controllers (PLCs). It was originally invented to describe logic made from relays. The name is based on the observation that programs in this language resemble ladders, with two vertical "rails" and a series of horizontal "rungs" between them           
SRC
StringToArray DST
STClosed "Structured text" A high-level language that is block structured and syntactically resembles Pascal           Q

ST Language

Q := StringToArray (SRC, DST);

See Also

ArrayToString / ArrayToStringU