Subtraction -

Operator - Performs a subtraction of all inputs.

Inputs

Input

Data Type

Range

Unit

Default

Description

IN1

ANY_NUM / TIME

 

 

 

First input.

IN2

ANY_NUM / TIME

 

 

 

Second input.

Outputs

Output

Data Type

Range

Unit

Description

Q

ANY_NUM / TIME

 

 

Result: IN1 - IN2.

Remarks

  • All inputs and the output must have the same type.

FBD Language

SubFbd.gif (1612 octets)

FFLD Language

  • In the FFLD language, the input rung (EN) enables the operation.
    • The output rung (ENO) keeps the same value as the input rung.
    • The subtraction is executed only if EN is TRUE.
    • ENO is equal to EN.

SubLd.gif (1477 octets)

IL Language

Op1: FFLD  IN1
     SUB IN2
     ST  Q    (* Q is equal to: IN1 - IN2 *)
Op2: FFLD  IN1
     SUB IN2
     SUB IN3
     ST  Q    (* Q is equal to: IN1 - IN2 - IN3 *)

ST Language

Q := IN1 - IN2;

See Also