Terminal

Overview

The terminal view provides a quick and easy way to issue commands to the drive directly. Typically used by "power users" who are familiar with the command set, the terminal view can help in setup, troubleshooting, and other diagnostic actions. When using the terminal view, WorkBench shows the parameter and command set in a popup view and uses an autocomplete tool to help you select the proper parameter or command. Right-click in the command entry area to open a pop-up menu for editing commands and for clearing the screen. The terminal also provides a macro editor that allows a series of commands to be executed via a single command (called a macro). Macros are useful when you must frequently execute a sequence of commands.

Using the Terminal

Select Terminal in the navigation tree to issue parameters and commands in the terminal view. You can enter parameters and commands at the prompt as shown in this example:

The terminal supports the following keyboard shortcuts:

Keyboard Shortcut Description

F2

Executes the last command.

Up Arrow

Gets the previous command from the command history.

Down Arrow

Gets the next command from the command history.

CTRL+J

Shows the list of commands that the drive supports.

CTRL+L

Opens the Parameter Load/Save view.

ESC

Hides the command list if command list is open. Clears the line if command list is not open.

Enter (Return)

Executes the current command. This command sends the text you have typed to the drive and then prints the text the drive returns on the next line.

Macros

Macros are a short sequence of instructions that can be sent to the drive using a single button. You can create up to five macros within the terminal view using the macro editor. Each of the macros will appear as a button below the terminal view. When you select the button, the command set tied to that macro will appear in the terminal view and the commands will be executed. If there are commands which are not entered correctly, the terminal view will indicate the errors.

You can access macros and the macro editor from the buttons located at the bottom of the terminal view. Select a macro button to execute the associated macro. The Edit Macros... button opens the macro editor used to create and edit macros. You can also assign custom names to the macro buttons with this editor.

Creating a Macro from Terminal Commands

You can create a macro from a sequence of terminal commands as follows:

1. Select Edit Macros..., and choose a macro to edit.

2. Enter a sequence of commands into the Commands window:

3. The macro is auto-saved. Select Close to return to the terminal view.

Macro Editor

The macro editor allows you to create and modify up to five macros.WorkBench automatically saves the macros that you create. If you exit WorkBench and then start WorkBench again, the macros you defined will still be available.

To create or edit a macro from the editor, open the Terminal view and select Edit Macros... (located at the bottom of the screen). Select the macro you wish to edit from the tree on the left, then use the features described below to build the macro. You can add comments in the macro after the ";" symbol.

Button or Dialog Box Description

Name

Allows you to give each macro a unique name. This name will be shown on the button in the terminal view.

Commands

Displays the commands that are sent to the drive when you use this macro. The response from the drive is displayed in the terminal.

Import

Overwrites the selected macro with the contents of a macro file exported from another computer.

Export

Sends the selected macro to a text file to that you can import into WorkBench running on another computer.

Insert Delay

Inserts a step into the macro that causes a delay for a specified number of milliseconds before continuing. A line that starts with #delay 5000 will pause the execution of the macro for 5000 milliseconds.

Close

Closes this window and returns to the terminal view.