MOVE.ABORT
Description
MOVE.ABORT stops motor motion and allows continued program execution. Deceleration is determined by CS.DEC.
-
-
MOVE parameters are only valid when DRV.OPMODE = 2 and DRV.CMDSOURCE = 5.
Example
This program segment commands the motor at constant velocity until input 1 goes to a logic 0. Then, the motor is commanded to stop.
MOVE.ACC = 5000
‘Set acceleration rate equal to 5,000 rpm/sec CS.DEC = 10000 'Set controlled stop deceleration rate to 10,000 rpm/sec
MOVE.RUNSPEED = 120
‘Set Run speed equal to 120 rpm
MOVE.GOVEL
When DIN2.STATE = 0, MOVE.ABORT 'Motor decelerates to a stop at CS.DEC (10,000 rpm/sec)
Print “Move Aborted!”
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1144 |
No | Command | No |
M_01-05-11-000 |
Related Topics