MOVE.SCURVETIME
Description
MOVE.SCURVETIME sets the amount of S-curve smoothing applied to all velocity profiles. The greater the value of MOVE.SCURVETIMEe, the smoother (lower jerk) the profile.
Specifying a non-zero value for MOVE.SCURVETIME increases move time by MOVE.SCURVETIME. For example, a trapezoidal move (MOVE.SCURVETIME = 0) that takes 0.500 seconds to complete, takes 0.756 seconds to complete if MOVE.SCURVETIME is set to 256.
Change this parameter only when the motor is not moving (MOVE.MOVING = 0). If you attempt to make a change while the motor is moving, an F826, "Cannot execute during a move" fault is produced.
-
-
MOVE parameters are only valid when DRV.OPMODE = 2 and DRV.CMDSOURCE = 5.
General Information
|
Type |
R/W |
|
Units |
Milliseconds |
|
Range |
0 to 512 (0, 0.5, 1, 2, 4, 8, 16, 32, 64, 128, 256, 512) |
|
Default Value |
0 |
|
Data Type |
Float |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1142 |
No | 32 bit | No |
M_01-05-11-000 |
Related Topics
MOVE.ACC | MOVE.DEC | MOVE.GOREL | MOVE.GOABS | MOVE.GOHOME | MOVE.GOVEL