VM.PGMERRORLIST

Description

VM.PGMERRORLIST returns a list of items (such as recently added parameters) being used in the downloaded BASIC program which the installed firmware does not support. When the drive returns Fault 831 (BASIC program is invalid), you can either:

1. Use VM.PGMERRORLIST to identify and remove unsupported calls to items.

or

2. Upgrade your firmware, and then re-compile, and re-download the BASIC program.

General Information

Type

R/O

Units

N/A

Range

N/A

Default Value

N/A

Data Type

N/A

Start Version

M_01-09-00-000

Variants Supported

This parameter is only supported on AKD BASIC drives.