VM.START
Description
VM.START starts program execution. Or if program execution was stopped with VM.STOP, VM.STARTstarts the program at the point it was stopped.
-
-
This keyword is executed when the continue icon is pressed in the Program view.
General Information
|
Type |
Command |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
N/A |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1156 |
No | Command | No |
M_01-05-11-000 |
Related Topics