EGEAR.PULSESOUT
Description
EGEAR.PULSESOUT is the number of position counts the motor moves for each EGEAR.PULSESIN number of encoder counts. EGEAR.PULSESOUT must be set more recently than EGEAR.RATIO in order to use exact electronic gearing.
General Information
|
Type |
R/W |
|
Units |
Position counts |
|
Range |
-32,768 to 32,767 |
|
Default Value |
1 |
|
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1072 |
No | 8 bit | Yes |
M_01-05-11-000 |
Related Topics
EGEAR.PULSESIN | EGEAR.RATIO |EGEAR.ON | FB2.SOURCE | FB2.ENCRES | FB2.MODE