MOVE.TARGETPOS
Description
MOVE.TARGETPOS specifies the target position for an absolute (MOVE.GOABS) move. MOVE.TARGETPOS is an absolute position referenced to the electrical home position (the position where PL.FB = 0).
Set MOVE.TARGETPOS before initiating a MOVE.GOABS.
-
-
MOVE parameters are only valid when DRV.OPMODE = 2 and DRV.CMDSOURCE = 5.
General Information
|
Type |
R/W |
|
Units |
Depends on UNIT.PROTARY or UNIT.PLINEARUNIT.ACCLINEAR Rotary: counts, rad, deg, (Custom Units), 16-bit counts Linear: counts, mm, µm, (Custom Units), 16-bit counts |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
Variants Supported
This parameter is only supported on AKD BASIC drives.
Fieldbus Information
|
Fieldbus |
Index/Subindex |
Is 64 bit? | Attributes | Signed? |
Object Start Version |
|---|---|---|---|---|---|
|
Modbus |
1146 |
Yes | 64 bit | Yes |
M_01-05-11-000 |
Related Topics