STRINGS.PHASELOSSOFTHRESH
Description
When a phase loss is detected, a fault (F541, F542, or F543) is triggered only if the string current is larger than the value of STRINGS.PHASELOSSOFTHRESH. Otherwise a warning is displayed.
General Information
Type |
R/W Parameter |
Units |
Arms |
Range |
0 to DRV.IPEAK |
Default Value |
8 Arms |
Data Type |
Float |
Start Version |
M_01-13-11-000 |
Variants Supported
Variant | Supported |
---|---|
AKD Base | No |
AKD with Position Indexer | No |
AKD EtherCAT | No |
AKD CANopen | No |
AKD BASIC | No |
AKD SynqNet | No |
AKD EtherNet/IP | No |
AKD PROFINET | No |
AKD Sercos® III | No |
AKD-N | No |
AKD-C | Yes |
*In SynqNet, a parameter may be available in the firmware but have no effect on the system. See SynqNet Supported Parameters.
Related Topics
The AKD-C Central Power Supply