Invalid Firmware
When WorkBench connects to a drive, it checks to make sure that the drive is executing a valid version of the drive firmware. If the drive is executing firmware earlier than version 1-01-00-000, then WorkBench cannot operate correctly and shows these options.
| Button | Description |
|---|---|
|
Download |
This command allows you to select a different version of the firmware and download it to the drive. |
|
Disconnect |
This command stops all communications with the drive and return to the disconnected state. |
See Also