AIN#.CUTOFF

Description

AIN#.CUTOFF sets the break frequency in Hz for two cascaded single-pole low-pass filters on the hardware command input. Since the two poles are cascaded at the same frequency, the -3 dB frequency is 0.64*AIN#.CUTOFF in hertz and the 10% to 90% step response rise time is 0.53/AIN#.CUTOFF in seconds.

Suggested operating values are as follows:

  • Analog torque opmode: 5 kHz
  • Analog velocity opmode: 2.5 kHz
  • General purpose analog input high resolution: 500 Hz

Examples

Context

For more information see Analog Input.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read/Write
Units Hz
Range 0 to 9998.638 Hz
Default Value 5001.216 Hz
Data Type Float
See Also  
Stored in Non-Volatile Memory Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AIN1.CUTOFF

3780h

02h

Unsigned32

-

1000:1

Read/Write

No

AIN2.CUTOFF

3781h

02h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

23000

1

23000 (0x59d8)

AIN1.CUTOFF

Unsigned32

Read/Write

Yes

23001

1

23001 (0x59d9)

AIN2.CUTOFF

Unsigned32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AIN1.CUTOFF

23000

Float

Read/Write

-

AIN2.CUTOFF

23001

Float

Read/Write

-