AOUT#.VALUE

Description

AOUT#.VALUE reads the analog output value.

Examples

Context

For more information see Analog Output.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type Read Only
Units V
Range 0 to 10V
Default Value 0V
Data Type Float
See Also  
Stored in Non-Volatile Memory No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AOUT1.VALUE

3800h

01h

Signed16

-

1000:1

Read only

Yes

AOUT2.VALUE

3801h

01h

Signed16

-

1000:1

Read only

Yes

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

24000

1

24000 (0x5dc0)

AOUT1.VALUE

Signed16

Read Only

Yes

24001

1

24001 (0x5dc1)

AOUT2.VALUE

Signed16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AOUT1.VALUE

24000

Float

Read Only

-

AOUT2.VALUE

24001

Float

Read Only

-