AXIS#.CANOPEN.CONTROLWORD
Description
Allows recording, triggering, and viewing the associated axis’ CANopen controlword. See 6040h.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-01-00-000 |
General Information
|
Type |
Read Only |
|
Units |
N/A |
|
Range |
N/A |
|
Default Value |
N/A |
|
Data Type |
Integer |
|
See Also |
Variants Supported
CAN bus drives: AKD2G-SPC
EtherCAT drives: AKD2G-SPE