AXIS#.FBUS.P

Description

This command allows reading the position set by fieldbus when in certain fieldbus modes.

Fieldbus Applicable Modes
EtherCAT Profile position
CAN Profile position
PROFINET MDI_POS signal
EtherNet/IP Position command when using command type 6 (position move) while AXIS#.OPMODE is position

  • Writing to this command is possible and is used when AXIS#.CMDSOURCE is fieldbus. Depending on the fieldbus mode, may be overwritten by the fieldbus.

Versions

Action Version Notes
Implemented 02-04-06-000

 

General Information

Type

Read/Write

Units

Rotary: counts, rad, deg, custom units, 16-bit counts

Linear: counts, mm, µm, custom units, 16-bit counts

See Position Units.

Range

Depends on units. See Position Range.

Default Value

0

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

Fieldbus variants: AKD2G-SPP, AKD2G-SPE, AKD2G-SPC

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5106

1

5106 (0x13f2)

AXIS1.FBUS.P

Signed32

Read/Write

Yes

70642

2

5106 (0x13f2)

AXIS2.FBUS.P

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.FBUS.P

5106

Signed32

Read/Write

Position