AXIS#.FBUS.V

Description

This command allows reading the velocity set by fieldbus when in certain fieldbus modes.

Fieldbus Applicable Modes
EtherCAT Profile position
CAN Profile position
PROFINET MDI_VEL signal
EtherNet/IP Velocity command when using command types 6 (position move) and 7 (jog) while AXIS#.OPMODE is position

  • Writing to this command is possible and used when AXIS#.CMDSOURCE is fieldbus. Depending on the fieldbus mode, may be overwritten by the fieldbus.

Versions

Action Version Notes
Implemented 02-04-06-000

 

General Information

Type

Read/Write

Units

Rotary: RPM, RPS, deg/s, (custom units)/s, rad/s

Linear: counts/s, mm/s, µm/s, (custom units)/s

See Velocity Units.

Range

Depends on units. See Velocity Range.

Default Value

0 RPM

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

Fieldbus variants: AKD2G-SPP, AKD2G-SPE, AKD2G-SPC

Industrial Ethernet Information

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5105

1

5105 (0x13f1)

AXIS1.FBUS.V

Signed32

Read/Write

Yes

70641

2

5105 (0x13f1)

AXIS2.FBUS.V

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.FBUS.V

5105

Float

Read/Write

Velocity