AXIS#.HOME.P
Description
AXIS#.HOME.P is the position given to the home point once it is found.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Rotary: counts, rad, deg, custom units, 16-bit counts See Position Units for details. |
|
Range |
Depends on units. See Position Range for details. |
|
Default Value |
0 |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.HOME.P |
5008h |
0fh |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS2.HOME.P |
5108h |
0fh |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS1.HOME.P |
607ch |
00h |
Signed32 |
Position |
- |
Read/Write |
No |
|
AXIS2.HOME.P |
687ch |
00h |
Signed32 |
Position |
- |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6109 |
1 |
6109 (0x17dd) |
AXIS1.HOME.P |
Signed32 |
Read/Write |
Yes |
|
71645 |
2 |
6109 (0x17dd) |
AXIS2.HOME.P |
Signed32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.HOME.P |
6109 |
Signed32 |
Read/Write |
Position |