AXIS#.HWEN.STATE

Description

This parameter returns the state of the hardware enable input.

If AXIS#.HWEN.SOURCE=0, indicating that no hardware enable input is configured, AXIS.HWEN.STATE always returns 1.

Usage

0: Hardware enable input is low preventing the axis from being enabled.

1: Hardware enable input is high allowing the axis to be enabled.

Versions

Action Version Notes
Implemented 02-00-00-000#  

General Information

Type Read Only
Units N/A
Range 0 to 1
Default Value N/A
Data Type Integer
See Also AXIS#.HWEN.SOURCE, AXIS#.HWEN.MODE

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.HWEN.STATE

5009h

03h

Unsigned8

-

-

Read only

No

AXIS2.HWEN.STATE

5109h

03h

Unsigned8

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

7002

1

7002 (0x1b5a)

AXIS1.HWEN.STATE

Unsigned8

Read Only

Yes

72538

2

7002 (0x1b5a)

AXIS2.HWEN.STATE

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.HWEN.STATE

7002

Unsigned8

Read Only

-