AXIS#.IL.DFB

Description

This parameter displays the measured, de-rotated d-component current value of the AXIS#.MOTOR. This parameter is commonly used with IPM motors (AXIS#.MOTOR.TYPE = 6), where the d-component current is controlled for closed loop current regulation.

Versions

Action Version Notes
Implemented 02-00-00-000

 

General Information

Type

Read Only

Units

Arms

Range

± Drive peak current (IPEAK)

Default Value

N/A

Data Type

Float

See Also

N/A

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported