AXIS#.IL.FOLDFTHRESHU
Description
AXIS#.IL.FOLDFTHRESHU is set by the user as the fault threshold of both motor and drive foldback algorithms. The actual threshold value, namely AXIS#.IL.FOLDFTHRESH , is the minimum of AXIS#.IL.FOLDFTHRESHU, AXIS#.IPEAK and AXIS#.MOTOR.IPEAK . Setting AXIS#.IL.FOLDFTHRESHU to zero will stop faults F2001 and F2017 from being generated.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Arms |
|
Range |
0 to 500 Arms |
|
Default Value |
Drive peak current (IPEAK) |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.IL.FOLDFTHRESHU |
500ah |
09h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
AXIS2.IL.FOLDFTHRESHU |
510ah |
09h |
Signed32 |
- |
1000:1 |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
5806 |
1 |
5806 (0x16ae) |
AXIS1.IL.FOLDFTHRESHU |
Signed32 |
Read/Write |
Yes |
|
71342 |
2 |
5806 (0x16ae) |
AXIS2.IL.FOLDFTHRESHU |
Signed32 |
Read/Write |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.IL.FOLDFTHRESHU |
5806 |
Float |
Read/Write |
- |