AXIS#.IL.LIMITN

Description

This parameter sets the negative user limit clamp value of the torque-producing q-component current command (AXIS#.IL.CMD). The current command is additionally limited by the motor peak current setting (AXIS#.MOTOR.IPEAK ) and by the present value of the foldback I²t peak motor current protection.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

A

Range

Negative drive peak current (IPEAK) to 0 A

Default Value

Negative drive peak current (IPEAK)

Data Type

Float

See Also

AXIS#.IL.LIMITP

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.IL.LIMITN

500ah

05h

Signed32

-

1000:1

Read/Write

No

AXIS2.IL.LIMITN

510ah

05h

Signed32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5813

1

5813 (0x16b5)

AXIS1.IL.LIMITN

Signed32

Read/Write

Yes

71349

2

5813 (0x16b5)

AXIS2.IL.LIMITN

Signed32

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.IL.LIMITN

5813

Float

Read/Write

-