AXIS#.MOTOR.BRAKEIMM

Description

Sets the brake to apply as soon as the power stage disables. The brake will not apply immediately when the disable command is issued, but at the point when the power stage actually disables. The power stage can disable due to user command (AXIS#.DIS ), digital input, fieldbus, STO, or fault. The point at which the power stage disables depends on the disable mode settings or type of fault for each case.

Value Description
0 Inactive
1 Brake as soon as power stage disables.

Context

For more information see Brake and Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 1

Default Value

0 (Inactive)

Data Type

Integer

See Also

N/A

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.BRAKEIMM

500bh

0dh

Unsigned8

-

-

Read/Write

No

AXIS2.MOTOR.BRAKEIMM

510bh

0dh

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6224

1

6224 (0x1850)

AXIS1.MOTOR.BRAKEIMM

Unsigned8

Read/Write

Yes

71760

2

6224 (0x1850)

AXIS2.MOTOR.BRAKEIMM

Unsigned8

Read/Write

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.BRAKEIMM

6224

Unsigned8

Read/Write

-