AXIS#.MOTOR.BRAKEPOWERDELAY

Description

Time to wait after applying full voltage before dropping to low voltage when AXIS#.MOTOR​.BRAKEPOWERSAVING = 1.

Context

For more information see Brake and Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

Milliseconds

Range

0 to 2000

Default Value

150

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.BRAKEPOWERDELAY

500bh

24h

Unsigned16

-

-

Read/Write

No

AXIS2.MOTOR.BRAKEPOWERDELAY

510bh

24h

Unsigned16

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6238

1

6238 (0x185e)

AXIS1.MOTOR.BRAKEPOWERDELAY

Unsigned16

Read Only

Yes

71774

2

6238 (0x185e)

AXIS2.MOTOR.BRAKEPOWERDELAY

Unsigned16

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.BRAKEPOWERDELAY

6238

Unsigned16

Read Only

-