AXIS#.MOTOR.BRAKEPOWERLOW
Description
Low voltage used by power saving brake operation (AXIS#.MOTOR.BRAKEPOWERSAVING).
-
-
This parameter is automatically configured for Kollmorgen motors when AXIS#.MOTOR.AUTOSET = 1 and motor memory version is 0.4 or greater. This parameter can be modified while AXIS#.MOTOR.AUTOSET = 1 if its AXIS#.MOTOR.DISAUTOSET index = 1.
Context
For more information see Brake and Motor.
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
Volts |
|
Range |
10.602 to 24.002 |
|
Default Value |
17 |
|
Data Type |
Float |
|
Stored in Non-Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Industrial Ethernet Information
|
Command |
Index |
SubIndex |
Data Type |
Units |
Float Scale |
Access |
PDO Mappable |
|---|---|---|---|---|---|---|---|
|
AXIS1.MOTOR.BRAKEPOWERLOW |
500bh |
25h |
Unsigned16 |
- |
1000:1 |
Read/Write |
No |
|
AXIS2.MOTOR.BRAKEPOWERLOW |
510bh |
25h |
Unsigned16 |
- |
1000:1 |
Read/Write |
No |
|
ID |
Instance |
Attribute |
Name |
Data Type |
Access |
User Mappable |
|---|---|---|---|---|---|---|
|
6239 |
1 |
6239 (0x185f) |
AXIS1.MOTOR.BRAKEPOWERLOW |
Unsigned16 |
Read Only |
Yes |
|
71775 |
2 |
6239 (0x185f) |
AXIS2.MOTOR.BRAKEPOWERLOW |
Unsigned16 |
Read Only |
Yes |
|
Parameter |
PNU |
Data Type |
Access |
Units |
|---|---|---|---|---|
|
AXIS#.MOTOR.BRAKEPOWERLOW |
6239 |
Float |
Read Only |
- |