AXIS#.MOTOR.LDLL

Description

This parameter is the motor line to line direct (flux producing) axis inductance.


  • This parameter is required to be configured for AXIS#.MOTOR.TYPE = 0, 1, 4, 6, and 8.

Context

For more information see Motor.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

mH

Range

1 to 2^31

Default Value

4

Data Type

Float

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.LDLL

500bh

28h

Unsigned32

-

1000:1

Read/Write

No

AXIS2.MOTOR.LDLL

510bh

28h

Unsigned32

-

1000:1

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6230

1

6230 (0x1856)

AXIS1.MOTOR.LDLL

Unsigned32

Read Only

Yes

71766

2

6230 (0x1856)

AXIS2.MOTOR.LDLL

Unsigned32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.LDLL

6230

Float

Read Only

-