AXIS#.MOTOR.RTYPE

Description

This parameter defines the type of thermal resistor inside the motor to measure motor temperature. The following resistor types are supported:

AXIS#.MOTOR.RTYPE Thermal Resistor Type
0 Single PTC
1 Single NTC
2 KTY83-110
3 KTY84-130
4 PTC + KTY83-110
5 Thermal switch
6 PTC + PT1000
7 Dual PTC
8 PT1000
127 No sensor

See Motor Temperature View.

Versions

Action Version Notes
Implemented 02-00-00-000

General Information

Type

Read/Write

Units

N/A

Range

0 to 8, 127

Default Value

0

Data Type

Integer

Stored in Non-Volatile Memory

Yes

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.MOTOR.RTYPE

500bh

19h

Unsigned8

-

-

Read/Write

No

AXIS2.MOTOR.RTYPE

510bh

19h

Unsigned8

-

-

Read/Write

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

6214

1

6214 (0x1846)

AXIS1.MOTOR.RTYPE

Unsigned8

Read Only

Yes

71750

2

6214 (0x1846)

AXIS2.MOTOR.RTYPE

Unsigned8

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.MOTOR.RTYPE

6214

Unsigned8

Read Only

-